Technical FAQs

Ask a Question

Does the HPALM handle padlock attachment lock the breaker in the ON or OFF position?

Yes, except on the MA, MAL, MH, MHL, ME, MEL, MX and MXL circuit breakers. where it will only lock in the OFF position. Where locking in the ON position is required for these breakers, use the HPAXLM padlock attachment and MAHEX handle extension together.

CTA-ID : 8807
Was this helpful?
What can we do to improve the information ?