Technical FAQs

Ask a Question

With an NA breaker, does it matter which side of the breaker accessories are installed on?

The alarm switch, shunt trip or undervoltage trip can be installed on either side, the auxiliary switch must be placed in the upper right pocket.


CTA-ID : 8781
Was this helpful?
What can we do to improve the information ?