Technical FAQs

Ask a Question

How much torque should be applied to the terminals on NA accessories?

The NA accessories will accept #18 to #12 control wires and should be torqued to 9 lb.-in. or 1 N-m.


CTA-ID : 8780
Was this helpful?
What can we do to improve the information ?