Technical FAQs

Ask a Question

Customer has an NA breaker and is going to install an NA11021 shunt trip. Which of the 4 terminals does he use?

All NA shunt trips use terminals 24 & 25.


CTA-ID : 8776
Was this helpful?
What can we do to improve the information ?