Technical FAQs

Ask a Question

Can you run two Altivar ATV66 drives with the same start stop and analog 10V signal for the speed reference?

The start stop is just as easy as relay contacts for the logic inputs. The AI2 can be run to both as long as the signal stays good and can supply enough mA for both inputs.


CTA-ID : 7202
Was this helpful?
What can we do to improve the information ?