Technical FAQs

Ask a Question

What is the maximium voltage specification for the R3 relay on the 24 volt Altivar ATV66 I/O card?

Told him that he can use 120 VAC at 2 Amps or 220 VAC at 1 Amp.


CTA-ID : 7197
Was this helpful?
What can we do to improve the information ?