Technical FAQs

Ask a Question

What is the speed regulation of the Altivar ATV66 with and with out the Tachometer feed back?

I told him that In Normal or High Torque the Speed regulation is 1.0 Percent and 0.5 Percent with optional Tachometer.

CTA-ID : 7194
Was this helpful?
What can we do to improve the information ?