Technical FAQs

Ask a Question

What is the peak inverse voltage value of the inputs from the bridge diode on the Altivar ATV66?

The continuous rating of the bridge is 1600V but the inverse peak will be a lot higher but I do not have that info.

CTA-ID : 7191
Was this helpful?
What can we do to improve the information ?