Technical FAQs

Ask a Question

Can a stored setting in the Altivar ATV58 keypad be downloaded to different hp rated drives?

No. The keypad can store up to 4 different files, but they can only be transferred to drives with the same part number and firmware revision level.
Refer to the keypad programming guide for additional details.


CTA-ID : 6893
Was this helpful?
What can we do to improve the information ?