Technical FAQs

Ask a Question

Why is the 2 seconds Timing relay required in series with the Shunt Trip Coil Relay on the Altistart ATS46 recommended wiring setup?

It allows some time for the fault relay to energize in the softstarter when the unit is powered up. This prevents tripping every time on start up.


CTA-ID : 7500
Was this helpful?
What can we do to improve the information ?