Technical FAQs

Ask a Question

Does the Altistart ATS46 unit electronically remember the thermal calculations it has monitored while running the motor?

Yes. There is a memory in the processor that knows the motor had been run in based on the current monitored it stores the required information upon a restart.


CTA-ID : 7492
Was this helpful?
What can we do to improve the information ?