Technical FAQs

Ask a Question

Can you set a logic input for fault reset on the Altistart ATS46?

Yes, parameter LI can be set to fault reset. It is a level 3 parameter. This will allow any resettable fault to be remotely reset.


CTA-ID : 7487
Was this helpful?
What can we do to improve the information ?