Technical FAQs

Ask a Question

Why do we say to use a output filter on cable lengths of 75 ft or greater and then for lager hp 300 ft or greater on Altivar ATV66.

We have tested the following lenghts and seen a higher DV/DT after exceeding the specified cable distance. These are just guidel lines; other factors can cause a higher DV/DT levels.

CTA-ID : 7177
Was this helpful?
What can we do to improve the information ?