Technical FAQs

Ask a Question

Is the output filter and the line reactor used on VSD07 the same device.

NO, the output filter prevents DV/DT at the motor. A line reactor is device that adds impedance to the line, this inturn reduces the distortion on the line and the current draw is lessened.

CTA-ID : 7176
Was this helpful?
What can we do to improve the information ?