Technical FAQs

Ask a Question

Is the output filter and the line reactor used on Altivar ATV56 the same device?

NO, the output filter prevents DV/DT at the motor. A line reactor is device that adds impedance to the line, this inturn reduces the distortion on the line and the current draw is lessened. The units are physically two different devices.


CTA-ID : 7173
Was this helpful?
What can we do to improve the information ?