Technical FAQs

Ask a Question

What is the torque requirement for the AL400LAT lug for the LA, LH, and Q4 circuit breakers?

375 lb-in (42 N-M)


CTA-ID : 6560
Was this helpful?
What can we do to improve the information ?