Technical FAQs

Ask a Question

What is the torque requirement for the AL400LH7 lug for the LA, LH, and Q4 circuit breakers?

300 lb-in (34 N-m)


CTA-ID : 6556
Was this helpful?
What can we do to improve the information ?