Technical FAQs

Ask a Question

What are the repair parts for a QO11624L125GRB, Series S01, Load Center?

Issue:
Previous design series repair parts

Product line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4054802209
Interior Trim - 4054507501
Interior Assembly - QO11624L125GRBI
Neutral Bonding Screw - 4028345850K
Main Lugs - QOL125
Interior trim mounting screw - 4020513001K
RB door mounting screw - 2142717161
Main circuit breaker and main lugs keps nut - 2342702001


CTA-ID : 6550
Was this helpful?
What can we do to improve the information ?