Technical FAQs

Ask a Question

Can the motor be slowed down a little with a Altistart ATS46 soft start?

The speed of the motor can not be adjusted on a softstart. The softstart can slow the motor down to 0 hz with a set decel time when stop command is given. Need a variable frequency drive if need to control the speed of the motor.

CTA-ID : 7472
Was this helpful?
What can we do to improve the information ?