Technical FAQs

Ask a Question

Can you communicate with the Altivar ATV66 drive using SyNet which is a Symax protocol?

Need a conversion module to convert Synet to Modbus or Modbus Plus in order to establish communications between Symax PLC and ATV66 Drive unit.

CTA-ID : 7158
Was this helpful?
What can we do to improve the information ?