Technical FAQs

Ask a Question

Why does the breaker in the Altivar ATV66 enclosuse trip when put the drive in bypass?

First thing need to do is adjust the setting on the breaker setting to correct value, factory set is MIN which is probably the issue. Next would want to confirm the amperage draw motor is pulling and make sure it is ok and not bound up.

CTA-ID : 7151
Was this helpful?
What can we do to improve the information ?