Technical FAQs

Ask a Question

Is there an option for a Smoke purge input with the 8839 enclosed Altivar ATV66, like there is on the ATV56?

The closes thing is the Q207 option which is the inhibit/shutdown sequence instantly (or Q208 for time delay). Then you should add in the engineering notes on the order how you want this to work.

CTA-ID : 7149
Was this helpful?
What can we do to improve the information ?