Technical FAQs

Ask a Question

What is the instruction bulletin number for the Altivar 28 drive?

It is a VVDED399062USR01/02.  This is available in the literature fullfillment center or on-line in the technical library.


CTA-ID : 6861
Was this helpful?
What can we do to improve the information ?