Technical FAQs

Ask a Question

Which wire sizes will terminate in the AL400LH7 and AL400H7T lug for the LA, LH, and Q4 circuit breakers?

350-750 kcmil (185-400 mm2)


CTA-ID : 6548
Was this helpful?
What can we do to improve the information ?