Technical FAQs

Ask a Question

Which wire sizes will terminate in the CU400LA lug for the LA, LH, and Q4 circuit breakers?

(1) #1 AWG-600 kcmil (50-300 mm2) or
(2) #1 AWG-250 kcmil (50-120 mm2)


CTA-ID : 6530
Was this helpful?
What can we do to improve the information ?