Technical FAQs

Ask a Question

Can you use single phase line power or a single phase motor on the Altistart ATS46 or the ATS48 units?

The ALTISTART 46 (ATS46) or the ATS48 Soft Start is a 3-phase device and is designed for control of standard three-phase asynchronous induction (squirrel cage) motors.
It is not designed to be used with single phase line power or single phase motors.


CTA-ID : 7468
Was this helpful?
What can we do to improve the information ?