Technical FAQs

Ask a Question

Can the thermal protection be turned off in Altistart ATS46?

Yes, thp can be set to off. Make sure that external thermal overload protection is provided to protect the motor.


CTA-ID : 7455
Was this helpful?
What can we do to improve the information ?