Technical FAQs

Ask a Question

Does the Altistart ATS46 softstart have Ground fault protection?

Issue: Does the Altistart ATS46 softstart have Ground fault protection?
 
Product Line: ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: No. There is no ground fault detection in the soft starter.


 
Was this helpful?
What can we do to improve the information ?