Technical FAQs

Ask a Question

What does the interposing ground fault relay do and does it come in the Altistart ATS46 8638 enclosed unit?

The ground fault relay monitors the current in the third leg of the input to the softstart, it provides an extra measure of protection against grounding, but this is a customer supplied option, we do not include it in the enclosed units.

CTA-ID : 7449
Was this helpful?
What can we do to improve the information ?