Technical FAQs

Ask a Question

Is Orient function available with the Altivar ATV66 drive?

The ATV66 offers an open loop type of Orient function with the VW3A66201T or VW3A66202T I/O Extension Modules.


CTA-ID : 7134
Was this helpful?
What can we do to improve the information ?