Technical FAQs

Ask a Question

Is it possible for the Altivar 58 drive to do serial communications using the keypad port?

Yes. The keypad port is Modbus port. However, it is not possible to use this port to communicate on a Modbus network and the keypad at the same time.


CTA-ID : 6851
Was this helpful?
What can we do to improve the information ?