Technical FAQs

Ask a Question

What is a 9007ASL1?

This is a member of the Point of Purchase, or POP, system. These are devices packaged in plastic clam shells to display on a peg board at a distributor. The 9007 ASL1 consists of a 9001 C54B2 and a 9007 MA11.


CTA-ID : 6501
Was this helpful?
What can we do to improve the information ?