Technical FAQs

Ask a Question

What is a 2510 K1?

This is a member of the Point of Purchase, or POP, system. These are devices packaged in plastic clam shells to display on a peg board at a distributor. The 2510 K1 consists of a 2510 KG2.

CTA-ID : 6499
Was this helpful?
What can we do to improve the information ?