Technical FAQs

Ask a Question

What is a 8910 D2?

This is a member of the Point of Purchase, or POP, system. These are devices packaged in plastic clam shells to display on a peg board at a distributor. The 8910 D2 consists of a 8910 DP21V02.

CTA-ID : 6498
Was this helpful?
What can we do to improve the information ?