Technical FAQs

Ask a Question

What is a 8910D1?

This is a member of the Point of Purchase, or POP, system. These are devices packaged in plastic clam shells to display on a peg board at a distributor. The 8910 D1 consists of a 8910 DP32V02.

CTA-ID : 6497
Was this helpful?
What can we do to improve the information ?