Technical FAQs

Ask a Question

What is included in a QOVP1 Load Center Value Pack?

Issue:
Product design features

Product Line:
QO load centers

Environment:
Value pak components

Cause:
application

Resolution:
The QOVP1 includes a QO13040M200C load center (with a combination cover), and 5 - QO120 branch circuit breakers


CTA-ID : 6492
Was this helpful?
What can we do to improve the information ?