Technical FAQs

Ask a Question

How do you program the InTele Braking in the Altistart ATS46?

In level 2 set the StY = b.
If necessary, adjust the praking torque level from 0 to 100% at the brc parameter in level 2.
Also, can adjust the braking time in level 3, parameter EbA.
See the VD0C32S301B manual for details.


CTA-ID : 7436
Was this helpful?
What can we do to improve the information ?