Technical FAQs

Ask a Question

What is the correct way to connect the control power to the ATS46?

The control circuit is completely independent of the power circuit. To select control voltage, follow the instructions on the label located on the top of the controller:
For 208-240 V: move terminal cover from position 230 to position 460/500 V and connect single phase voltage supply to terminals C and 230 V.
For 380-415 V: move terminal cover from position 400 to position 460/500 V and connect single phase voltage supply to terminals C and 400 V.
For 440-500 V: check that exposed control terminals are marked C and 460/500 V. If not, move blue terminal cover from 460/500 V terminal and connect single phase voltage supply to terminals C and 460/500 V.


CTA-ID : 7429
Was this helpful?
What can we do to improve the information ?