Technical FAQs

Ask a Question

What is the largest size Altivar ATV66 unit you can obtain before have to get enclosed unit instead of open style?

Informed that above size 6 units then all of the drives are in enclosures but for size 6 down which is ATV66C15N (200hp) or lower can get open.

CTA-ID : 7122
Was this helpful?
What can we do to improve the information ?