Technical FAQs

Ask a Question

Why can`t the customer order a 3-15 PSI follower option with power circuit K with the Altivar enclosed ATV66, especially since he can order it with the ATV56?

It must be due to enclosure size with the line isolation contactor, because it is only with the smaller drives in combination with the power circuits with the line isolation contactor that this is not acceptable.


CTA-ID : 7121
Was this helpful?
What can we do to improve the information ?