Technical FAQs

Ask a Question

What is the duty rating of the DB resistors for the Altivar ATV66 drives?

The resistors are rated for continuous current, so they can be pulsed at the rated current continually.


CTA-ID : 7118
Was this helpful?
What can we do to improve the information ?