Technical FAQs

Ask a Question

Is the dynamic braking circuit on the Altivar ATV66 protected thermally?

Yes, the dynamic braking circuit will open up when the temperature is too hot


CTA-ID : 7116
Was this helpful?
What can we do to improve the information ?