Technical FAQs

Ask a Question

What are the LEMs on the Altivar ATV66?

Informed that the LEMs are the motor current sensors used on the drive to monitor current levels.


CTA-ID : 7114
Was this helpful?
What can we do to improve the information ?