Technical FAQs

Ask a Question

Will replacing an Altivar ATV66 control basket version 2.1 with 3.2 version Control basket fix problem having with drive going back to default settings sometimes when power is cycled to the unit?

Yes, the 2.1 version software had that possible problem but the 3.2 version software will fix it.

CTA-ID : 7112
Was this helpful?
What can we do to improve the information ?