Technical FAQs

Ask a Question

Does the Altistart ATS46 - Enclosed 8839 NRA4R meet requirements for service entrance?

Told him if you are talking about three phase and ground connections, then YES. If you are talking about interrupt rating, the molded case switch is only rated 35K amps and may not be.


CTA-ID : 7425
Was this helpful?
What can we do to improve the information ?