Technical FAQs

Ask a Question

Is the setup memory on the Altistart ATS46 unit volatile or non-volatile memory?

The setup is saved to EEPROM memory. The starter reads setup when powered up. The settings are saved to non-volatile memory.


CTA-ID : 7416
Was this helpful?
What can we do to improve the information ?