Technical FAQs

Ask a Question

Why does the display go to ``8.8.8`` and you here a relay toggling when try to start the Altistart ATS46?

Per Mike Montgomery, it would be same issue that was seen on the ATV16 drive when see ``888`` on display, the (SMPS) switch mode power supply has a problem so would need to replace the control head of the softstarter.

This fault is undocumented in literature under the list of faults.

CTA-ID : 7415
Was this helpful?
What can we do to improve the information ?