Technical FAQs

Ask a Question

Can circuit breakers be used as a disconnect means on the ATS46?

Yes, the chart to chose the correct breaker is on p27 of VD0C32S301B instruction bulletin. See attachment.


CTA-ID : 7410
Was this helpful?
What can we do to improve the information ?