Technical FAQs

Ask a Question

Would it be ok to substitute the line fuses with GV2s on the Altivar ATV66 because customer does this with AB units and we also have a GV2 as the disconnect on our enclosed ATV58 package and don`t recommend fusing?

Even though the GV2 does have current limit characteristics we do not recommend substituting them for the line fuses because the line fuses are what we tested unit with to get the ratings described.


CTA-ID : 7106
Was this helpful?
What can we do to improve the information ?