Technical FAQs

Ask a Question

What can be done to prevent Altivar ATV66 units from tripping on overvoltage and phase fault when capacitors are switching on line?

May want to consider placing a detuning reactor on cap bank, will detune to the 4th harmonic so that they cancel out, or a precharge circuit on the cap bank. They already have 5% reactors on the system.

CTA-ID : 7104
Was this helpful?
What can we do to improve the information ?